Post Go back to editing

Loop filter for HMC440 and HMC733 (sythentiser and VCO respectively)

Thread Summary

The user inquired about the HMC440 application circuit, specifically the choice of opamp, biasing voltage, and LDO/regulator options. The support engineer confirmed that the LT6200 family is a suitable alternative to the THS4031, and a single +10V bias can be used instead of dual ±5V. For the LDO, the LT3045 is recommended, or direct connection with decoupling capacitors can be used.
AI Generated Content
Category: Datasheet/Specs
Product Number: HMC440; HMC733

I refer to the application circuit above from the datasheet of the HMC440 and will like to know the following:

1. I tried the several filters in ADsimPLL and the LT6200 seems to give the best phase noise performance. Is this a good choice of OpAmp or is a design as above limited to the THS4031 opamp as active filter?

2. Instead of the +/-5V for biasing the opamp, can I use a single bias of +10V and GND?

3. Any suggestions of a LDO or regulator that can be used with the opamp?

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.