Hello everybody,
I am developing a simple signal generator from 100 MHz to 1 GHz and stumbled on these two PLL chips. They are pin compatible so for my first test i used the wider option the MAX2870. I build a custom PCB and successfuly connected the chip with my MCU (STM32) and made a simple program to set sweep frequency range and execute. This all is working well and im quite happy with it. However i would like to ask this forum with some help because i want to push the MAX2870 (or ADF4351 i dont really care which one will be used if it will solve my issue) as far as possible in order to obtain to smallest step size possible. Generally i would be happy if i could change the frequency in 100Hz steps. I dont know if this is possible or not but if yes then even lower 10 Hz step would be ideal. What have i tried is to lower the PFD frequency but lowering it below 6.25MHz makes the PLL unresponsive. Can somebody help me what to improve to obtain this kind of resolution ? Can anybody help me with loop filter optimisation and clock setup to obtain the 100 or even 10 Hz step size ?
Thank you.