| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | Closed | |
ADL9005
Recommended for New Designs
The ADL9005 is a gallium arsenide (GaAs), monolithic microwave integrated circuit (MMIC), pseudomorphic high electron mobility transistor (pHEMT), wideband...
Datasheet
ADL9005 on Analog.com
ADL9006
Recommended for New Designs
The ADL9006 is a gallium arsenide (GaAs), pseudomorphic high electron mobility transistor (pHEMT), monolithic microwave integrated circuit (MMIC), low...
Datasheet
ADL9006 on Analog.com
HMC998APM5E
Production
The HMC998APM5E is a GaAs pHEMT MMIC Distributed Power Amplifier which operates from DC to 22 GHz. The amplifier provides +15 dB of gain, +42 dBm output...
Datasheet
HMC998APM5E on Analog.com

Hi Jorge,
With regard to the HMC998APM5E, VGG1, must always be applied first. VGG1, VDD, VGG2is power sequence required to safely bias up the amplifier. If the 12 V is applied first, the HMC998APM5E will be damaged.
When powering down the HMC998APM5E turn of VDD first, followed by VGG2 and last turn of VGG1.
Regards,
Jim B
Hi Jorge,
Based on what I see from your bias sequence, indicated by the red number, seem to be fine within your block diagram. Keep in mind that ADL9005 and HMC998 are going to need a bias tee on the output RFOUTVDD1 to operate the drain voltage and a blocking cap at the input as well.
Regards,
Dorant