Post Go back to editing

multiple ADF4368 synchronization

Thread Summary

The user inquires about using ADF4368 for frequency hopping with two PLLs in a phased array application, asking if multiple eval boards can handle the test and if a single ACE GUI can manage them. The final answer suggests using the DC2609A eval board with LTC6952, which can be used by disabling the PLL and on-board VCO, and is compatible with TimeSync and EZSync. The HMC7043 is also mentioned as an alternative for generating SYNC signals, but it is not compatible with TimeSync and EZSync. The accompanying answers clarify that the DC2610A eval board is not currently available but will be stocked, and that a single pulse can be generated by configuring the LTC6953 outputs via SPI commands.
AI Generated Content
Category: Hardware
Product Number: ADF4368

Hi,

I plan to use ADF4368 for frequency hopping with two PLLs mux (ping-pong). I want to take advantage for ADF4368’s built-in “EZSync” and “Phase Resynchronization” functions for phased array applications. The rough block diagram is shown as below. To experiment this concept, do you think multiple eval boards can handle this or I need a special custom test board for it? If mulitple EVBs can handle this kind of test, does single ACE GUI handle this or need separate individual GUI per EVB needed?  If you have some instructions for multiple EVBs, can you please advise? Also, if you already have the test boards similar like this, can you please let me know if I can buy some?

Thanks

Parents
  • Hi  

    You can build an experimental setup with two ADF4368 evaluation boards and one LTC6953 evaluation board to test the synchronization feature. ACE GUI can handle multiple sessions, so you can connect all evaluation boards to the same computer with ACE Software.

    You can connect the two ADF4368 evaluation boards and the LTC6953 board as shown in the below diagram. You can distribute both reference clocks and SYNC signals using the LTC6953 EZsync feature. 

    The below video can give an idea about the Dual ADF4368 configuration with LTC6953.

    Synchronizing Multiple Fractional PLLs | Analog Devices

    Here is the proposed block diagram for the Dual ADF4368 operation shown in the video. We haven't released the board yet. Unfortunately, I don't know the release timeline. 

    Thanks,

    Emrecan

Reply
  • Hi  

    You can build an experimental setup with two ADF4368 evaluation boards and one LTC6953 evaluation board to test the synchronization feature. ACE GUI can handle multiple sessions, so you can connect all evaluation boards to the same computer with ACE Software.

    You can connect the two ADF4368 evaluation boards and the LTC6953 board as shown in the below diagram. You can distribute both reference clocks and SYNC signals using the LTC6953 EZsync feature. 

    The below video can give an idea about the Dual ADF4368 configuration with LTC6953.

    Synchronizing Multiple Fractional PLLs | Analog Devices

    Here is the proposed block diagram for the Dual ADF4368 operation shown in the video. We haven't released the board yet. Unfortunately, I don't know the release timeline. 

    Thanks,

    Emrecan

Children
  • Hi Emrecan,

    Thank you for the information in detail. I could not find DC2610A (LTC6953 Eval Board) at all. Will is be stocked someday? Can you please advise where can I buy them? Or, if you can recommend other distributor with the phase sync function, please recommend one.

    Best,

    Youngho

  • Hi Youngho,

    DC2610A is an active evaluation board and it should be stocked soon. I'll ask around internally what the latest status is.

    The DC2609A evaluation board is in stock on Digikey. This board contains LTC6952. LTC6952 is an LTC6953 with a PLL. You can use this board by disabling the PLL and on-board VCO. It is also compatible with TimeSync and EZSync.

    We have another clock distributor part named HMC7043; however, the minimum input frequency of HMC7044 is 400MHz. If your reference frequency is suitable, HMC7043 can provide SYNC signals and reference distribution.

    HMC7043 is not compatible with TimeSync and EZSync. The only way to sync ADF4368 is to use the SYNC input of ADF4368.

  • Hello Emrecan,

    Thanks for the alternative part info. About SYNC signal from LTC6953 to ADF4368, if this is a need base single triggering pulse, how do we manage this pulse with trigger with LTC6952 or LTC6953 since they just produces a series continuous pulses? 

    Best,

  • Hi,

    You can generate a desired number of pulses by writing an SPI command or external trigger.  The most straightforward way to produce a single pulse is to set LTC6953 outputs as pulse output and trigger pulse generation using the SPI command. You can select the number of pulses to be created via SPI.

    Thanks,
    Emrecan