Post Go back to editing

MAX2021 baseband Output Differential Impedance (Demodulator)

Thread Summary

The user inquired about the baseband output impedance of the MAX2021 when used as a demodulator, noting that the datasheet only specifies the input impedance as 53 ohms. The final answer directed the user to contact Maxim Integrated's technical support for assistance, as Maxim products are not supported on EngineerZone.
AI Generated Content
Category: Hardware
Product Number: MAX2021
Software Version: Not applicable

The MAX2021 datasheet specifies the baseband input differential impedance when the part is used as a modulator as 53 ohms (page 3, very first line in table).  However, nowhere in the datasheet does it specify the baseband output impedance when used as a demodulator.  Can you confirm that it is the same 53 ohms?  Or please specify how to treat this demodulator property.  Thank you.