KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
HMC738
Recommended for New Designs
The HMC738 is a GaAs InGaP Heterojunction Bipolar Transistor (HBT) MMIC VCO. The HMC738 integrates a resonator, negative resistance device, varactor diode...
Datasheet
HMC738 on Analog.com
HMC699
Recommended for New Designs
The HMC699LP5(E) is a frequency synthesizer with a wideband reversible polarity digital PFD and lock detect output. The divider operates from 160 - 7000...
Datasheet
HMC699 on Analog.com
ADF5000
Recommended for New Designs
The ADF5000 prescaler is a low noise, low power, fixed RF divider block that can be used to divide down frequencies as high as 18 GHz to a lower frequency...
Datasheet
ADF5000 on Analog.com
I am working on a project that needs to produce 40.5 GHz for molecular spectroscopy reasons. As such, I planned on using your HMC738 to generate 20.25 GHz, and then double the frequency using a standard diode doubler.
While I am able to generate these tones, I have not been able to remove what appears to be noise humps at roughly +/- 50 kHz from the nominal signal. I have already tried the following, with results listed as applicable. I'm running out of ideas to check, and would appreciate any guidance you can offer. If additional information would be helpful, please advise.
Original Schematic:



Changes to Schematic in debugging:

Layout:

Layout (zoomed-in):

Stackup:

Current output spectrum:
Debugging attempts:
Please let me know what other results I can provide. If I don't figure this out, I'll be forced to respin with a lower frequency VCO (starting at 10.125 GHz, then multiplying by 4). It is my present hope that this noise hump behavior will be less likely if I use a VCO operating at a more reasonable "Kv" tuning sensitivity, as using HMC738 at 20.25 GHz forces operation at the peak VCO sensitivity region.
Hi,
Just to confirm, are you using the HMC699 for the PLL? I see in the schematic that the ADF5000 is used. I assume in SimPLL the HMC699 is used as the ADF5000 is not in the SimPLL library?
As a debug test could you isolate multiplier and check if the direct VCO ~20GHz output has the same 50kHz bump.
A phase noise plot would also be of benefit if you can share this.
Thanks,
Kieran
Hi Kieran,
Thanks for replying - yes, I'm using HMC699 as the main PLL, with ADF5000 providing external prescaling.
The uploaded picture details are small, but I've already verified that the direct VCO 20.25 GHz has the 50 kHz bump (uploaded spectrum analyzer is centered at 20.25 GHz - bump content is effectively identical at 20.25 GHz & 40.5 GHz). Are you suggesting that I should try physically removing the multiplier entirely? I'd have to struggle with improvising a high frequency bypass if I still wanted to probe the output.
I'll to upload phase noise plots this week.
Thanks,
Michael
Yes it would be useful to try to isolate just the PLL circuit without the multiplier to ensure there is no coupling occurring. If possible can the supplies be applied externally by a clean PSU to see if this changes anything?
Ok - I removed the X2 multiplier, and when probing the 20.25 GHz tone capacitively above the board, the noise humps remain very clear, so it appears to be either largely or completely independent of VCO load impedance.

The voltage supplies are currently provided from outside the board using low noise power supplies, and then locally regulated further down with standard LDO regulators. My experience suggests if we try to just use external supplies, we'll get more noise due to capacitive pickup then any we'd save by potentially using lower noise regulators. As such, I'm hesitant to try this approach, especially because I cannot measure noticeable noise on the internal voltage supplies.
Kieranb, your other suggestion turned out to be basically correct. While the voltage supplies were not explicitly oscillating, their noise was found to contribute to these humps on the RF carrier (in combination with the high sensitivity of the VCO, which is mostly a function of the frequency selection at 20.25 GHz). I was able to drive down the hump amplitude by ~20 dBc with more aggressive voltage regulator filtering, which should be enough for my current project.
That's good. I'm glad to hear this has now been resolved.
Thanks,
Kieran
I recall using an active loop filter a long time ago and had issues with excess noise within the loop bandwidth due to the opamp have a too low gain-bandwidth product. I see the opamp's GBW is only 330kHz or thereabouts. Try find an opamp with GBW 100x the loop bandwidth.