Post Go back to editing

ADPA1107 Gate Bias

Thread Summary

The user is working with the ADPA1107 in a pulsed drain configuration and needs a stable -2.7V gate bias. Switch-mode DC-DC converters are causing excessive switching noise (250mV peak-to-peak). The recommended solution is to use a low-noise LDO, specifically the LT3093, to achieve a cleaner and more stable bias voltage. The user is also considering the power supply driving the DC-DC converter as a potential source of noise.
AI Generated Content
Category: Hardware
Product Number: ADPA1107

Working with the ADPA1107 in a pulsed drain configuration. I need to create a -2.7V bias for the gate. 

Is there a recommended way to achieve this bias voltage and have it as stable as possible?

Thus far I have been trying to do this with a switch-mode DC-DC converter however the switching noise is a problem. The current supply I am using has at best about 250mV (peak to peak) of switching noise. I am worried that this will be a problem in operation as  there is only a small margin for the gate bias before it reaches its "off" condition. Also will the switching noise damage the amplifier? or will the RF gain become a function of these voltage transients?

Thanks

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.