Post Go back to editing

ADPA1107 Gate Bias

Thread Summary

The user is working with the ADPA1107 in a pulsed drain configuration and needs a stable -2.7V gate bias. Switch-mode DC-DC converters are causing excessive switching noise (250mV peak-to-peak). The recommended solution is to use a low-noise LDO, specifically the LT3093, to achieve a cleaner and more stable bias voltage. The user is also considering the power supply driving the DC-DC converter as a potential source of noise.
AI Generated Content
Category: Hardware
Product Number: ADPA1107

Working with the ADPA1107 in a pulsed drain configuration. I need to create a -2.7V bias for the gate. 

Is there a recommended way to achieve this bias voltage and have it as stable as possible?

Thus far I have been trying to do this with a switch-mode DC-DC converter however the switching noise is a problem. The current supply I am using has at best about 250mV (peak to peak) of switching noise. I am worried that this will be a problem in operation as  there is only a small margin for the gate bias before it reaches its "off" condition. Also will the switching noise damage the amplifier? or will the RF gain become a function of these voltage transients?

Thanks

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.