Post Go back to editing

Regarding LT5537 s1p file to simulate the input matching network and RF input vs output voltage

Thread Summary

The user requested simulation files to validate the performance of the TCM1-33WX+ transformer with the LT5537 log detector, specifically to plot RF input power vs output DC voltage. The support engineer provided a simulation showing good matching with a 100 Ohm resistive load, an insertion loss of ~1dB, and a voltage gain of 3dB. The engineer also suggested designing a matching network and simulating the RF voltage at the detector input, noting the LT5537's 20mV/dB slope.
AI Generated Content
Category: Hardware

Hello support team,

My requirement is to use TCM1-33WX+ 1:2 transformer with 100 ohm resistor at the input of LT5537 log detector . In order to validate the performance of TCM1-33WX+ balun with the LT5537 log detector, Is it possible from your end to provide S1P file or any other simulation file , so  that it will be possible for us to simulate RF input power vs output DC voltage mapping with this transformer and matching network?

Awaited your quick and positive response. 

Parents Reply Children
No Data