Post Go back to editing

Regarding LT5537 s1p file to simulate the input matching network and RF input vs output voltage

Category: Hardware

Hello support team,

My requirement is to use TCM1-33WX+ 1:2 transformer with 100 ohm resistor at the input of LT5537 log detector . In order to validate the performance of TCM1-33WX+ balun with the LT5537 log detector, Is it possible from your end to provide S1P file or any other simulation file , so  that it will be possible for us to simulate RF input power vs output DC voltage mapping with this transformer and matching network?

Awaited your quick and positive response. 

Parents Reply
  • Hello, 

    But I need to simulate LT5537 input matching network having TCM2-33WX+ Balun and plot a graph of Vout vs input power at different frequency sweep of 35-60 MHz.

    Is there any way to do this, because using S1P , it is only possible to check S11. but I want to figure out its effect on deviation on Vout vs input power?

    Request you to provide guidance for the same.

Children