Post Go back to editing

Alternatives to ADN2880 or HMC799

Category: Hardware
Product Number: ADN2880, HMC799

We are looking for a transimpedance amplifier with >700MHz bandwidth and low noise / high gain (10kOhm). The HMC799 would have appropriate specs but it is no available anymore (last time buy), PHY1095 the same, the ADN2880 has more BW than needed but could maybee work - but it is also not available anymore. The question is: Why are all the high speed transimpedance amplifiers gone? What would be the suggested alternative? The newer products (LTC656x, MAX4066x, MAX4065x, ...)  are to slow.