KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADN2880
Obsolete
The ADN2880 is a 3.3 V, high gain SiGe transimpedance amplifier (TIA). The TIA converts the small signal current of a photo detector into differential...
Datasheet
ADN2880 on Analog.com
HMC799
Last Time Buy
The HMC799LP3E is DC to 700 MHz Transimpedance amplifier designed for opto-electronic laser sensor applications, FDDI receivers and receiver systems employing...
Datasheet
HMC799 on Analog.com
PHY1095
Not Recommended for New Designs
The PHY1095 is a transimpedance amplifier designed for use within small form factor fiber optic modules targeted at gigabit-enabled passive optical network...
Datasheet
PHY1095 on Analog.com
HMC7992
Recommended for New Designs
The HMC7992 is a general-purpose, nonreflective, 0.1 GHz to 6.0 GHz, silicon, single-pole, four-throw (SP4T) switch in a
leadless, surface-mount package...
Datasheet
HMC7992 on Analog.com
LTC6563
Recommended for New Designs
The LTC6563 is a low-noise four-channel transimpedance amplifier (TIA) with 600MHz bandwidth. The LTC6563 TIA’s low noise, wide linear range, and low...
Datasheet
LTC6563 on Analog.com
LTC6269-10
Recommended for New Designs
The LTC6268-10/LTC6269-10 is a single/dual 4GHz FET-input operational amplifier with extremely low input bias current and low input capacitance. It also...
Datasheet
LTC6269-10 on Analog.com
We are looking for a transimpedance amplifier with >700MHz bandwidth and low noise / high gain (10kOhm). The HMC799 would have appropriate specs but it is no available anymore (last time buy), PHY1095 the same, the ADN2880 has more BW than needed but could maybee work - but it is also not available anymore. The question is: Why are all the high speed transimpedance amplifiers gone? What would be the suggested alternative? The newer products (LTC656x, MAX4066x, MAX4065x, ...) are to slow.
I see the HMC799 is in stock, but not out of stock
The HMC7992 is in stock, which is a completely different IC, some distributors seem to have problems with this...
The HMC7992 is in stock, which is a completely different IC, some distributors seem to have problems with this...