KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
ADN2880
Obsolete
The ADN2880 is a 3.3 V, high gain SiGe transimpedance amplifier (TIA). The TIA converts the small signal current of a photo detector into differential...
Datasheet
ADN2880 on Analog.com
HMC799
Last Time Buy
The HMC799LP3E is DC to 700 MHz Transimpedance amplifier designed for opto-electronic laser sensor applications, FDDI receivers and receiver systems employing...
Datasheet
HMC799 on Analog.com
PHY1095
Not Recommended for New Designs
The PHY1095 is a transimpedance amplifier designed for use within small form factor fiber optic modules targeted at gigabit-enabled passive optical network...
Datasheet
PHY1095 on Analog.com
HMC7992
Recommended for New Designs
The HMC7992 is a general-purpose, nonreflective, 0.1 GHz to 6.0 GHz, silicon, single-pole, four-throw (SP4T) switch in a
leadless, surface-mount package...
Datasheet
HMC7992 on Analog.com
LTC6563
Recommended for New Designs
The LTC6563 is a low-noise four-channel transimpedance amplifier (TIA) with 600MHz bandwidth. The LTC6563 TIA’s low noise, wide linear range, and low...
Datasheet
LTC6563 on Analog.com
LTC6269-10
Recommended for New Designs
The LTC6268-10/LTC6269-10 is a single/dual 4GHz FET-input operational amplifier with extremely low input bias current and low input capacitance. It also...
Datasheet
LTC6269-10 on Analog.com
We are looking for a transimpedance amplifier with >700MHz bandwidth and low noise / high gain (10kOhm). The HMC799 would have appropriate specs but it is no available anymore (last time buy), PHY1095 the same, the ADN2880 has more BW than needed but could maybee work - but it is also not available anymore. The question is: Why are all the high speed transimpedance amplifiers gone? What would be the suggested alternative? The newer products (LTC656x, MAX4066x, MAX4065x, ...) are to slow.
Hi,
I am moving this thread to RF and Microwave community. Someone there should be able to assist you.
Thanks,
Gilbeys
Hi,
Could you please check LTC6563? It can provide 600MHz bandwidth with 0.5pF photodiode capacitance
LTC6563 Datasheet and Product Info | Analog Devices
Depending on your photodiode capacitance, you may also try photodiode wizard and discrete op-amps to find a suitable solution
Photodiode Circuit Design Wizard | Analog Devices
Thanks
We have a 2pF photodiode, the LTC6563 is in the 300MHz region with this input capacitance.
The Photodiode Circuit Design Wizard is only working in the 100 to 400M range, the LTC6269-10 is the best discrete solution ADI has to offer and unfortunately it is not quite able to reach this performance level.
I see the HMC799 is in stock, but not out of stock
The HMC7992 is in stock, which is a completely different IC, some distributors seem to have problems with this...