Post Go back to editing

HMC8500 : strong compression of positive half-wave

Category: Hardware
Product Number: HMC8500

I am testing the HMC8500 AD eval board with CW sinewave at 330 MHz, Vdd = 28V, Vgg = -2.3V, Iddq = 100mA, load = 50Ohm :

- -4dBm / input -> 15.5dBm / output : slight compression of positive half wave

- 2dBm / input -> 21dBm / output : significant compression of positive half wave

- 7dBm / input -> app. 25dBm / output : very strong compression of positive half wave

I was expecting a nice sinewave output - especially at these low power levels.

Where is my misunderstanding of this device ?

I.e., can I not achieve symmetric output voltages at Pout >> 20 dBm ?

Parents
  • Hi Benlumentum,

                                  HMC8500 is fabricated using Gallium Nitride, (GaN). GaN devices exhibit a soft compression characteristic. So, the gain rolls off earlier than GaAs devices do. Refer to Figures 29 thru 33 in the HMC8500PM5E datasheet. This soft gain compression is shown.

    Regards,

    Jim B

  • Thank you, Jim, for the hints.

    But its only the positive half-wave which is heavily compressed. The negative follows the gain of the datasheet.

    Example below : @330 MHz,  7dBm / input -> app. 25dBm / output

    - Positive half-wave = 4.8Vp

    - Negative half-wave = 6.3Vp

    At low power levels, all looks fine.

    But if I go to higher power levels, this asymmetry gets worse and worse.

    Picture below  is 2V / DIV & 1ns / DIV. Scope BW = 1.3 GHz

      Vdd = 28V, Vgg = -2.3V, load = 50Ohm

      Iddq = 100mA (RF off)

      Idd = 120 mA (RF ON)

    Best regards,

    Marco

  • Hi Marco,

                     It is caused by the device starting to compress. The asymmetry is just how this device behaves.

    Regards,

    Jim B

Reply Children
No Data