Post Go back to editing

HMC4069 Lock Detect

Category: Hardware
Product Number: HMC4069

With the HMC4069 PLL IC, would there be any problem pulling the lock detect pin up to 3.3V, instead of the 5V supply, to make it compatible with 3.3V logic?  (The IC would still be powered from 5V.)

Parents
  • Hi,

    sorry for the delay in getting back to you. 

    I believe I responded to you through the FAE, but I write the response anyway here:

    I looked at the data sheet and that LD pin is an output, so if the pull up is at 5V or 3.3V depends on what you want to put as a receiver on that pin. If you put an LED, then the current that LED needs will determine the pull up voltage and the resistor value

    Petre

Reply
  • Hi,

    sorry for the delay in getting back to you. 

    I believe I responded to you through the FAE, but I write the response anyway here:

    I looked at the data sheet and that LD pin is an output, so if the pull up is at 5V or 3.3V depends on what you want to put as a receiver on that pin. If you put an LED, then the current that LED needs will determine the pull up voltage and the resistor value

    Petre

Children
No Data