Post Go back to editing

MAX2112 synthesizer/VOC manual setting・minimum Input frequency step

Category: Hardware
Product Number: MAX2112

Hi, I'm considering MAX2112.
I have three questions.

(1) I set the input frequency on the GUI of the MAX2112EVKIT.
Synthesizer settings, VCO selection and oscillation frequency are automatically set. How can I set these items manually?

(2)What is the minimum frequency step for the MAX2112EVKIT?
"Can I set it in 1Hz steps?"

(3)Do you have data on the device variation (average of gain for each voltage, standard deviation, etc.) for the graph of Input power vs. GC1 temperature characteristics?


Best regards, 

Yuya

Edit Notes

Add question
[edited by: Yuya at 12:28 AM (GMT -4) on 4 Jul 2023]
Parents Reply Children
No Data