Post Go back to editing

Requesting for S2P Files

Thread Summary

The user requested S2P files for HMC438, HMC433, HMC575, and an ADS/IBIS model for HMC698. S2P files are not available and cannot be generated. The IBIS model for HMC698 is being requested and will be provided if available. HMC438 works with sine wave input and has a typical output power of -1dBm, regardless of the input signal level. The combination of HMC438 and ADCLK needs to be set up to validate phase noise, as no simulation tools are available for this purpose. The differential output impedance of HMC438 is not specified in the thread.
AI Generated Content
Parents Reply
  • Also how should i simulate and check the combination of HMC438 and ADCLK? are there any specialized tools available? Because i need to see the phase noise of the ADCLK output. How should i validate it?

    2) The outpower level mentioned in HMC438 data sheet is typical -1dBm. Does that mean the loss will be 1dB or no matter what is the power level of input signal, the output will be -1dBm? 

    The same doubt for HMC433 aswell

Children
  • Hi,

    Yes, HMC438 works on sine wave input.

    As for the simulator, we do not have an available tool to check the phase noise of the combination of HMC438 and ADCLK. This combination needs to be setup to validate phase noise.

    Lastly, the -1dBm is the typical output power of HMC438 no matter what the power level of the input signal is supplied. Take note that there is a specified maximum input power for each input frequency range. The same goes for HMC433.

    Best regards,
    Mark

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.