Post Go back to editing

Requesting for S2P Files

Parents Reply Children
  • Also how should i simulate and check the combination of HMC438 and ADCLK? are there any specialized tools available? Because i need to see the phase noise of the ADCLK output. How should i validate it?

    2) The outpower level mentioned in HMC438 data sheet is typical -1dBm. Does that mean the loss will be 1dB or no matter what is the power level of input signal, the output will be -1dBm? 

    The same doubt for HMC433 aswell

  • Hi,

    Yes, HMC438 works on sine wave input.

    As for the simulator, we do not have an available tool to check the phase noise of the combination of HMC438 and ADCLK. This combination needs to be setup to validate phase noise.

    Lastly, the -1dBm is the typical output power of HMC438 no matter what the power level of the input signal is supplied. Take note that there is a specified maximum input power for each input frequency range. The same goes for HMC433.

    Best regards,
    Mark