MAX1473
Production
The MAX1473 fully integrated low-power CMOS superheterodyne receiver is ideal for receiving amplitude-shift-keyed (ASK) data in the 300MHz to 450MHz frequency...
Datasheet
MAX1473 on Analog.com
Dear,
We are looking for a replacement for the TDA5210 from Infineon for 433MHz and 868MHz.
We have seen the MAXIM MAX1473 device for the 433MHz band.
Do you think that this component can be suitable?
Is there a component in 868MHz with the same pin/out ?
Are there any other ISM components that might interest us?
Here are our requirements:
- Operating frequencies 434 and 868MHz
- ASK or OOK modulation
- If possible management of the superheterodyne mode.
- Application notes with preamp and saw filter for the different components
- The component must provide a DATA OUT demodulation pin for data reception.
- If the component requires programming of its registers before use, are they memorized in flash? or must the component be re-programmed after each power-up?
- We have 2 types of transmission protocol :
o A proprietary protocol at 1Kbps
o A Manchester type protocol at 10kbps
The particularity is that we have to manage the 2 speeds with the same component settings.
Thanks
Best regards
Hi RVB,
Maxim Integrated products are not supported on EngineerZone at this time. Below, I have included the technical support site where you can get assistance for Maxim Integrated products.
EN - https://maximsupport.microsoftcrmportals.com/en-US/tech-support/
Regards,
Dorant