Post Go back to editing

ADRF5720 unstable attenuation when using parallel mode

Thread Summary

The user experienced unstable attenuation and incorrect operation when using the ATTEN3/SEROUT pin, despite keeping PS low and toggling LE high. The final answer suggests checking if the part is damaged by verifying correct currents from the supply and control pins, testing in other modes, and trying different attenuation states. The power-up sequence is not considered the cause of the issue.
AI Generated Content
Category: Hardware
Product Number: ADRF5720

I just kept PS low, however the ATTEN3/SEROUT pin kept high, and when I toggled high LE,attenuation couldn't be changed correctly, however it was quite unstable. I wonder if it is because I didn't use a series 1 kΩ resistor to limit the current flowing in to the control pin, or I powered up VSS and VDD at the same time.

  • Hi ZhangZhongli

    Thanks a lot for the question. At first glance, your application issue is unrelated with the power-up sequence. However, it is always good practice to follow the recommended sequence and use case.

    I've got points you could check if the part is operating correctly.

    1) Could you read correct currents from the supply and control pins as described in the datasheet? If currents are incorrect, it is highly probable that the part is damaged.

    2) Were you be able to operate the part in any other mode (parallel/ serial)? If not so, could you try the simplest option?

    3) Is any other attenuation state work in your application? If you haven't tried, could you try couple?

    Gokhan