Post Go back to editing

Wideband Mixer under <2 GHz

Category: Hardware
Product Number: LTC5548

Dear Mr./Mrs,

I would like to ask, if you have a solution for a Mixer working from RF/LO 100MHz - 2 GHz (can be more), with IF output also 100-2GHz, but I need to work with that in whole frequency range, but every IC which I have opened needs matching for certain frequency. Maybe you do not have this solution. For higher frequencies I am using LTC5548 and need something for lower band. I have separate synthetiser in my design so do not need integrated.

I hope that my question is clear.

Thank you for answer.

Parents Reply Children
No Data