Post Go back to editing

LT5560 oscillator

Category: Hardware
Product Number: LT5560

Hello, we would like to replace discontinued product SA602AD (from NXP). I checked your website, compare your products and I think that best choice is the mixer LT5560, because it has lower quiescent current that other. I would like to ask you if you have any recommendation for an oscillator in fixed frequency with low power? 

It will be use in fixed 45MHz RF input frequency of mixer,  output frequency of mixer will be 10.7MHz (fixed too). So I need LO input 55.7MHz or 34.3MHz oscillator. Do you have any recommendation for connection with 3rd overtone crystal or something similar? SA602 has this oscillator circuit:

 


I could use ADF4360-9 (I use in other project) but the ADF4360-9 have high quiescent current and I need something lower (And ADF4360-9 has frequency band 65-400MHz). Is it possible use for example TCXO crystal oscillator with clipped sinus wave output? 

Thanks, best regards. Tomas.