Post Go back to editing

MAX2871 EVB Question

Thread Summary

The user needs to control MAX2871 devices on EVB-Kits without modifying the PIC controller. The final solution involves keeping the PIC in RESET mode and driving the control pins via the 20-pin INTF2400 connector, avoiding the need to reverse-engineer the USB communication protocol.
AI Generated Content
Category: Hardware
Product Number: MAX2871EVKIT

Hello,

For one of our new projects we need several MAX2871 devices. Due to the fact that we currently
are not able to buy these devices , we decided  buy the last 4 available EVB-Kits from our distributor.
For our development breadboards , we thought we could simply disconnect the PIC controller
and connect the PLL control signals to out own controller.

Unfortunately it seems it is not that simple without destroying the EVB. I would like to keep
the EVB-KITs as they are.

My question is, is the USB communication protocol between the PC-Software and
KIT available? In this case we could possibly convert our own serial signals into a
USB connection to control MAX2871KITs. It is complicated but it would keep the KITs.

Can anybody help please?

Thank you

-

Thread Notes