Post Go back to editing

LTC5598 - DC155A 5MHz to 1600MHz High Linearity Direct Quadrature modulator-Current rating issue

Category: Hardware
Product Number: LTC5598

Dear Sir,

I'm working in DC155A 5MHz to 1600MHz High Linearity Direct Quadrature modulator of LTC5598 chip. Initially, we gave supply voltage 5v if enable is high we get the current 240mA (typ- 165mA) and if enable is low we get 300uA (type-240uA) kindly suggest to me if can we proceed with the same current or not.



edited title to include product
[edited by: Dorant at 2:32 PM (GMT -5) on 20 Jan 2023]
Parents Reply Children
No Data