Post Go back to editing

HMC1019ALP4E -Thermal resistance (theta-JC)

Category: Hardware
Product Number: HMC1019ALP4E

Dear AD support,

I am looking for the junction thermal resistance at the board in the digital attenuation HMC1019ALP4E, however I would like some help to understand the following values?

The thermal resistance 143.5 °C/W corresponds to the junction-to-board or junction-to-case (top)?

The derated 6.8 mW/°C correspond to the junction-to-board ? For the the thermal analysis when can I use this value?

Thank you for your help,

Claudio

Edit Notes

updated titled with product
[edited by: Dorant at 4:25 PM (GMT -5) on 18 Jan 2023]
  • Hi CladioPC

    Thanks for the question and apologies for the late reply.

    Significant portion of the excess heat (more than ~95%) are transferred through the exposed paddle. Thermal resistance is from junction to the exposed paddle of the package.

    The continuous power dissipation spec is referenced to the package ground pad. The derating of Pdiss occurs for every degree C above 85 ambient you are operating the device at.

    The process technology and reliability limits may vary from part to part. As long as a good thermal relief is provided by the PCB, maximum operating temperature should be OK to use.

    Note that defining the case depends on package itself:

    - If package has exposed(visible) ground paddle, ground paddle is actually case
    - If package does not have exposed(visible) ground paddle but visible lead, lead is actually case.

    Thanks

    Gokhan