Post Go back to editing

TINYRAD - Can the FMCW timing of the DemoRad be altered?

Thread Summary

The user inquired about modifying the FMCW timing parameters, such as chirp repetition interval and chirp duration, on the DemoRad 1.2.0 platform. The final answer indicated that the DemoRad does not support these modifications due to ADC limitations. The engineer suggested using the EV-RADAR-MMIC2 platform, which has better ADC performance and can be configured for more precise timing, and provided references to articles on building 24 GHz FMCW radar systems and micro-Doppler studies.
AI Generated Content
Category: Software
Product Number: 24ghz Demorad 1.2.0 Version
Software Version: DemoRadTool-x32.exe

Hi,
Can the FMCW timing of the DemoRad be altered?

If not,what should I do to be able to configure the relevant timing parameters including chirp repetition interval and chirp duration?

Version: Demorad 1.2.0 


regards,
Tai J

Edit Notes

included EV_TinyRAD within the title
[edited by: Dorant at 3:28 PM (GMT -5) on 10 Jan 2023]