Post Go back to editing

ADL8121 - IP2 testing method

Category: Hardware
Product Number: ADL8121

Please describe the testing setup for the IP2 data shown in the plot below. For example, at 8GHz, are two tones near 4GHz applied as inputs, or are two tones near 8GHz applied? And is the sum frequency used as the output tone?



Updated title to include Product
[edited by: Dorant at 5:07 PM (GMT -5) on 4 Jan 2023]
Parents Reply Children
No Data