Hello,
I am simulating the ADL5569 with the provided 4 port S-parameters.
As a starting point, I am evaluating the ADL5569 common mode stability with the Stability Factor and the Stability measurement factor https://edadocs.software.keysight.com/display/genesys2009/Stability+Factor+and+Measure
For unconditional stability, the stability factor should be larger than 1 and the stability measurement factor larger than 0.
Between 2.4 GHz and 3.4 GHz, it is not case! Therefore, in this frequency range, the ADL5569 is potentially unstable.
Is it something you are aware of or is there something wrong with the S-parameters you are providing ?
Regards.
Nicolas