Hello Community,
as mentioned in the subject I am trying to bias the HMC863ALC4 with the HMC980LP4E. I tested the functions of the HMC980 and they seem to work as expected without any amplifier connected.
I could measure:
V_drain ~= 6V
V_gate = +2.8V (if EN high)
V_neg = -2.44V
V_gate = V_neg (if EN low)
V_dd = 6.04V
Now even though the HMC863 is connected there are no changes to the voltages.
Below you can see the schematics of both HMC980 and HMC863.
The diode D1 is a Schottky-diode as on the eval board (BAT54SLT1G). So that's not a problem.
I also checked if the current limiter of the power supply kicks in, but that's neither the case.
Would really appreciate your help.
Regards
Jan