Post Go back to editing

adf5901 output power stability

Category: Hardware
Product Number: ADF5901
Software Version: -

Hello Madam/Sir,

I am working with ADF4159-ADF5901-ADF5904 chips to perform FMCW radar application. I have observed that when I use 100us up and down chirp with 250 MHz sweep bandwidth, I am observing that the output power of ADF5901 is stable during 1.4 ms. What I mean by this is that ADF5901 transmits chirps (7*200us) with stable output power and after that time output power is changing almost 0.5to1dB. This issue continues periodically with a period of 1.4 ms. 

I wonder what the reason for that will be

1. Is there a periodic calibration in ADF5901 after initialization?

2. Is there a way to keep output power stable from chirp to chirp?

3. Is there a limit for output power stability?

4. Do you have any suggestions for us to fix the issue?

 

Best regards,

Ersin