Post Go back to editing

ADL5902 About input power

Category: Datasheet/Specs
Product Number: ADL5902

Page21 For the graph in Figure 46, the measurement conditions listed in the comments below the graph include
Figure 46 Output Noise, Rise and Fall Times vs. CLPF Capacitance, Single-Carrier W-CDMA (TM1-64) at 2.14 GHz with PIN = 0 dBm
 and it states that 0 dBm is input, but the description below that states
 However, the explanatory text below that states that the input is 0 dBm.
Figure 46 also shows how CLPF affects the response time of VOUT.
To measure this, an RF burst at 2.14 GHz at -10 dBm was applied to the ADL5902.
 To measure this, an RF burst at 2.14 GHz at -10 dBm was applied to the ADL5902.
Which is the correct input level (0 dBm or -10 dBm) for Figure 46?

Translated with www.DeepL.com/Translator (free version)