KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
HMC346
Obsolete
The HMC346 devices are absorptive, voltage variable attenuators (VVAs) operating from dc to 8 GHz, 14 GHz, 18 GHz, or 20 GHz. They feature on-chip reference...
Datasheet
HMC346 on Analog.com
Dear ADI support,
Can the HMC346AMS8G switch be used with 0/+5V control voltage by connecting the ground paddle and ground pins to +VDD and DC blocking the RF input / output pins?
If so, is there any anticipated problem with RF performance aspects such as return loss, distortion or insertion loss / isolation?
Any precautions when doing this? Thank you,
Jerry
6.8 GHz. Yes the ground paddle, pins would be at +5V, the RF pins DC blocked. The concern was mainly about return loss degradation if this mode of operation was functional.
The I-V2 loop aims for return loss optimization for any arbitrary V1 voltage in the default operation. In the shifted operation, if you observe unacceptable return losses, you may tune the impedance correction loop maybe.
You may sweep the 500ohm resistor to 400 or 600ohms maybe
The I-V2 loop aims for return loss optimization for any arbitrary V1 voltage in the default operation. In the shifted operation, if you observe unacceptable return losses, you may tune the impedance correction loop maybe.
You may sweep the 500ohm resistor to 400 or 600ohms maybe