Hi all,
The hmc447 is not working properly on my board when 26G input and 5V power are well supplied,there is a large signal output at 5Ghz around when i checked the output.And the signal is hung and moved which is like self-oscillation.What's worse, the part will no longer work normally when this happen.That menas i have to replace it with a new part if i want to get to work properly.
I have some questions about hmc447:
1.Does it need a DC-blocked capacitor when there is a hmc519 before hmc447? i see the output of hmc519 is DC blocked internally from the datasheet,so i didn't add a dc capacitor at the input in my design.
2.when the hmc447 worked abnormally,i checked the input impedance of hmc447 which is 1.5 ohm instead of 50 ohm.Which may cause this happen?
Thanks.