Post Go back to editing

Does MAX2830 support 2.4GHz frequency band, ASK modulation?

Thread Summary

The user inquired about the suitability of the MAX2830, MAX2831, and MAX2832 for developing a proprietary ASK protocol in the 2.4GHz frequency band. The final answer indicated that Maxim branded products are not supported within the forum and directed the user to the official Maxim support portal for further assistance.
AI Generated Content
Category: Datasheet/Specs

I have a project that needs to develop a proprietary protocol in the 2.4GHz frequency band, and the modulation method is ASK; I wonder if the MAX2830 can meet the requirements of RF transceiver? Similarly, can MAX2831 and MAX2832 models meet the requirements? Or can other series products meet the needs?