Hi! I want to use the AD8367 to realize the AGC function together with the AD8361. The reference circuit shown in Fig.38 shows the coupling between the output of AD8367 and the input to AD8361 is simply based on the series resistor R1(200kR). I am wondering due to the input impedance of AD8361's RFIN port, will the voltage at RFIN pin be attenuated and rather small since the resistor divider? Can you explain the circuit adopted here? And what's the best and most propriate way to realize the coupling between main signal path and the path for RMS detection? Thanks for your help!
Best,
Haojie Wu