Category: Hardware
Product Number: AD8318 ADL5330
I want to design an AGC loop as described in datasheet of the ADL5330.
I have two questions:
1-) AGC loops need a VGA, a detector and a comparator. As can be seen from the datasheet, there is no comparator to be used for AGC loop.
Is it only populating ADL5330 and AD8318 enough to construct an AGC loop?
2-) Bandwidth of the AD8318 is very wide which is from 1MHz to 8GHz.
But I want to only measure 20MHz bandwidth around 1.5GHz.
Is there a setting for AD8318 to adjust its bandwidth since I do not want to use additional SAW filters?