Post Go back to editing

AD8318 Broadband Temperature Sensitivity with Constant R_TADJ

Category: Hardware
Product Number: AD8318

What ist the temperature sensitivity of the AD8318 at 3.6 GHz and 5.8 GHz with the R_TADJ resistor having 500 Ohms?

In the datasheet, the temperature sensitivity at 3.6 GHz and 5.8 GHz  is only specified with R_TADJ of 51 and 1000 Ohms respectively.

We want to use the AD8318 over its full frequency range without adjusting the Resistor R_TADJ, if possible.

I assume the best broadband temperature sensitiviy is achieved by setting R_TADJ to 500 Ohms?

Parents Reply Children
No Data