AD8339
Production
The AD8339 is a quad I/Q demodulator configured to be driven by a low noise preamplifier with differential outputs. It is optimized for the LNA in the...
Datasheet
AD8339 on Analog.com
Dear Reader,
We are having trouble installing the SPI/USB software for the AD8339 Evaluation board.
The install folder has these files:
> AD8339 SPI2.msi, 12/13/2018
> AD8339.pdf, 12/16/2018, Rev B
> setup.exe, 12/13/2018
We have attempted the run "setup.exe" on four computers, with two .NET errors:
(1) Installing on two established Windows 10 Notebooks produced this error:

(2) Installing on a fresh Windows 10 notebook produced this error:

Initially clicking [Yes] browsed to a missing web page at Microsoft.
Repeated clicks on [Yes] installed the latest version of .NET
Despite installation for latest .NET, setup repeated the above Error
Is .NET 2.0 beyond Microsoft "End of Life"?
(3) Installing on an established Windows 7 produced the same error as (1), above.
How do we install the Eval Software on Windows 10?
> Do we need a new version, etc?
> What are the work-around options?
> We need the board to work as soon a possible
Thanks,
Dave