KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
November Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Ever wonder how EMC limits came to be and why they matter? Dive into the interesting bits of EMC limits and levels, then test your knowledge with EMC: The Interesting Bits Quiz.
Read the blog first: EMC Limits and Levels Explained: Well, the Interesting
View All
AD8339
Production
The AD8339 is a quad I/Q demodulator configured to be driven by a low noise preamplifier with differential outputs. It is optimized for the LNA in the...
Datasheet
AD8339 on Analog.com
Dear Reader,
We are having trouble installing the SPI/USB software for the AD8339 Evaluation board.
The install folder has these files:
> AD8339 SPI2.msi, 12/13/2018
> AD8339.pdf, 12/16/2018, Rev B
> setup.exe, 12/13/2018
We have attempted the run "setup.exe" on four computers, with two .NET errors:
(1) Installing on two established Windows 10 Notebooks produced this error:

(2) Installing on a fresh Windows 10 notebook produced this error:

Initially clicking [Yes] browsed to a missing web page at Microsoft.
Repeated clicks on [Yes] installed the latest version of .NET
Despite installation for latest .NET, setup repeated the above Error
Is .NET 2.0 beyond Microsoft "End of Life"?
(3) Installing on an established Windows 7 produced the same error as (1), above.
How do we install the Eval Software on Windows 10?
> Do we need a new version, etc?
> What are the work-around options?
> We need the board to work as soon a possible
Thanks,
Dave
Hi Dave,
The AD8339 software was initially created for Windows XP, but if a Windows XP machine isn't readily available, I have had success with using a Windows XP VM and installing that software on the VM. That allowed me to program the AD8339 through the VM that had Windows XP.
Additionally, the AD8339 SPI interface is a very simple 20-bit shift register interface (no addresses) plus a latch so you should be able to use a generic SPI controller with the AD8339.
Regards,
Dan