HMC424ALH5
Production
The HMC424ALH5 is a broadband 6-bit GaAs MMIC digital attenuator housed in a hermetic SMT leadless package. Covering DC to 13 GHz, the insertion loss is...
Datasheet
HMC424ALH5 on Analog.com
HMC441LC3B
Production
The HMC441LC3B is an efficient GaAs PHEMT
MMIC Medium Power Amplifier housed in a leadless
RoHS compliant SMT package. Operating between
6 and 18 GHz,...
Datasheet
HMC441LC3B on Analog.com
hello
I am designing the RF part of the transmitter chain shown in the figure below. The signal level measured from the modulator's output ranges of -30 dBm. This design aims to amplify this signal and deliver variable power in the range of 37-40 dBm to the antenna. To achieve this goal, HMC3587LP3BE amplifiers have been used as gain blocks; the driver amp is HMC441LC3B and also qorvuqpa1011 is used as the power amplifier. In this chain, an HMC424ALH5 stepped attenuator has been used to change the power level. Since this stepped attenuator has an acceptable attenuation resolution, Is the use of this attenuator in this scheme justifiable?
Your drawing indicates that the input frequency is 8 GHz. HMC424 is specified to operate form dc to 3 GHz. So you are going to need a higher frequency attenuator. I'm not sure of your question "is the use of this attenuator in this schematic" justifiable. From a signal balancing perspective, I would probably move the attenuator more to the center of the signal chain. There are models for all of these components in ADIsimRF (you can make a custom model for the Qorvo part). The software allows you to do frequency and DSA attenuation sweeps (www.analog.com/adisimrf)
Hi enash
thank you for replying
but based on the datasheet of HMC424 this IC worked in 8 GHz to 13 GHz
HMC424AG16 is specified from DC to 3 GHz. HMC424ALH5 is specified from DC to 13 GHz. I'm surprised that two parts with the same root part number (HMC424) have such different frequency ranges. Anyway, if you use HMC424ALH5, then it will, as you say, cover your 8 GHz operating frequency.
HMC424AG16 is specified from DC to 3 GHz. HMC424ALH5 is specified from DC to 13 GHz. I'm surprised that two parts with the same root part number (HMC424) have such different frequency ranges. Anyway, if you use HMC424ALH5, then it will, as you say, cover your 8 GHz operating frequency.