Post Go back to editing

HMC439 use as frequency Comaprison

Thread Summary

The user wants to compare two frequencies using the HMC439 and a loop filter without a VCO. The support engineer suggests this is not the intended use and may introduce hysteresis, recommending a mixer or the AD8302 for frequency comparison. The AD8302 can measure phase difference, but the user needs to convert frequency difference to phase difference for accurate measurement.
AI Generated Content
Category: Software
Product Number: hmc439

Hi, I want to use HMC439 and Loop Filter to compare two frequencies. I do not want to use VCO. 

The idea is to input two different frequencies to HMC439 then use a loop filter and read the output voltage of loop filter to draw the comparison between the input frequencies.

Can i do it using HMC439 because in doing so, i will not be using VCO and hence loop is not closed.

Parents Reply
  • Dear Aandrews, AD8032 can measure the phase difference between +- 90degrees. How can i convert the my frequency difference into phase difference?

    Lets say my Reference is 100MHz and my input frequency is 130MHz. Difference is 30MHz so how many degrees will correspond to 30MHz difference?

Children
No Data