Post Go back to editing

HMC439 use as frequency Comaprison

Thread Summary

The user wants to compare two frequencies using the HMC439 and a loop filter without a VCO. The support engineer suggests this is not the intended use and may introduce hysteresis, recommending a mixer or the AD8302 for frequency comparison. The AD8302 can measure phase difference, but the user needs to convert frequency difference to phase difference for accurate measurement.
AI Generated Content
Category: Software
Product Number: hmc439

Hi, I want to use HMC439 and Loop Filter to compare two frequencies. I do not want to use VCO. 

The idea is to input two different frequencies to HMC439 then use a loop filter and read the output voltage of loop filter to draw the comparison between the input frequencies.

Can i do it using HMC439 because in doing so, i will not be using VCO and hence loop is not closed.

Parents Reply
  • Thank you Aandrews.

    The output of mixer will be an IF frequency and i want a DC Voltage so i think mixer cannot be used.

    One more thing i want to ask is Lets say my Reference is 100 MHz and Input Frequency varies from 130 to 140 MHz. Will i be able to detect error voltage change as input frequency changes with 1MHz step

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.