I want to use Spartan 6 FPGA to give digital data directly to I & Q port of EVAL-ADRF6704 board.
In datasheet you have used DAC to give input, Is it necessary to use DAC?
Can we give digital data directly to I and Q port?
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
November Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Ever wonder how EMC limits came to be and why they matter? Dive into the interesting bits of EMC limits and levels, then test your knowledge with EMC: The Interesting Bits Quiz.
Read the blog first: EMC Limits and Levels Explained: Well, the Interesting
View All
ADRF6704
Obsolete
The ADRF6704 provides a quadrature modulator and synthesizer solution within a small 6 mm × 6 mm footprint while requiring minimal external components...
Datasheet
ADRF6704 on Analog.com
I want to use Spartan 6 FPGA to give digital data directly to I & Q port of EVAL-ADRF6704 board.
In datasheet you have used DAC to give input, Is it necessary to use DAC?
Can we give digital data directly to I and Q port?
Hi Anubhav,
you can use differential I/Q signals with correct DC bias from 400mV to 600mV.
Are you having any issue to get RF output signals?
Thanks
thanks for your response.
I wanted to make sure that the component can be used with FPGA before buying it.
My question is , With 0.5 v DC bais can i apply digital signal(square pulse) of 1v pp to I/Q port.
Ex. Vmin = 0.5v and vmax = 1.5 v to Ip.
In datasheet DAC provide current of 0mA to 20mA, Do I need to supply this amount of current or this modulstor IC can work with low current as well.
Can you please answer these two questions.
Hi Anubhav
0 to 20mA is a programmable current in DAC device and its purpose is to generate 0.5V common mode voltage. ADRF6704 datasheet doesn't say details on the input port except impedance plot in Figure 14. I also checked out similar device ADRF6755 and its datasheet says that 240uA current flow from the input ports and it indicates that input inside device has PNP configurations so in that case, common digital output port can't be connected to it. I am going to find the designer to figure out for ADRF6704.
in general ADRF6705 can fit DAC outputs and if the square waveforms are input, I am not sure how much harmonics are generated.
I am very great full of your response .
I wanted to operate at 2.7 GHz so ADRF6755 is not a good choice but Thank you for the recommendation.
So if can provide 0.5 dc bais common mode voltage to both inputs plus the data signal then i am good to go right?
please let me know the harmonic response of Square pulse so that i can start experimenting.
Thank you
Hi Anubhav
I talked to the designer and it might be possible to drive I/Q input ports by general purpose I/O (GPIO), but we have not tested such kinds of conditions. Unfortunately I don't have test set-up to inject digital square pulse at I/Q format with me so I can not provide harmonic degradation levels with the digital input case.
thank you for your support.