Post Go back to editing

About RF Amplifier ADPA1107

Category: Software
We require an RF Amplifier Evaluation board which supports 4GHz to 6GHz frequency with the output power of around 45dBm(35W). We need such an RF Amplifier board which is supported by TP-Link CEP510 or any ready product available from market which has output power 23dBm and will give input power 23dBm to the RF Amplifier board(ADPA-1107)
Is it possible to apply 23dBm input power to the RF Amplifier ADPA-1107 and which gives the output power around 45dBm(35W) ?
The UFL male connector is the output terminal of TP-Link CEP510. So is it supported to use UFL female to SMA male for the input to the RF Amplifier(ADPA-1107) ? We need connector compatibility.

Edit Notes

Added part number to title
[edited by: aandrews at 12:29 PM (GMT -4) on 5 May 2022]