Post Go back to editing

How to set the register of HMC1032 to use it in integer mode?

Thread Summary

The user encountered issues with the phase noise graph for the HMC1032, which did not match the datasheet when set to integer mode with a 10 MHz reference and 250 MHz output. The final answer suggested using the HMC830 model for simulation, as ADIsimPLL does not support the HMC1032. The user confirmed that this solution worked.
AI Generated Content

Hi, 

I set the registers to get 250 MHz output for integer mode, shown below. My reference is 10MHz.  However, I could not get the integer phase noise graph same as that in the datasheet of HMC1032. The phase noise I measured is more looks like fractional mode one. Which registers should I write to set it as an integer mode? Except Reg 06h[11] = 0. Reg 06h[7] = 1. 

Here is my INIT:

hwr 0x0A 0x2045
hwr 0x0B 0xFC061
hwr 0x02 0x1
hwr 0x06 0x307CE
hwr 0x09 0x3264

hwr 0x05 0xF88
hwr 0x05 0x6310
hwr 0x05 0x2898
hwr 0x05 0x60A0
hwr 0x05 0x1628
hwr 0x05 0x7FB0
hwr 0x05 0x0

hwr 0x03 0x96

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.