Post Go back to editing

The RF signal amplitude output of HMC264LC3B.

The RF signal amplitude output of f HMC264LC3B is too low, which is 20dB lower than that of subharmonic.

you can see RF signal at 26.05GHz(-47.56dBm) when LO=13GHz (-4dBm), IF = 0.05GHz (-8.44dBm) .

But the amplitude of subharmonic(26GHz) is -20dBm.