Post Go back to editing

ADF4159 Phase Coherence Between the chirp

Thread Summary

The user is seeking phase coherence between consecutive ramps using a single ADF4159 PLL in sawtooth burst mode. The support engineer explains that due to the fractional N sigma delta modulator (SDM), achieving phase coherence is difficult and may be impossible without external phase measurement and manual adjustment using the phase adjust controls.
AI Generated Content

Hello,

We are using ADF4159 for ramp generation and we require phase coherence between the ramps. means phase of start freq of ramp should be phased matched with next ramp start frequency phase.

Kindly help me to make this with ADF4159 PLL.

Regards

Sushant

Parents
  • Due to the fractional N sigma delta engine that the ramp generation uses, this is quite difficult maybe even impossible.

    See here for more detail

     Phase consistency between two ADF4159/ADF4169 PLLs 

  • Dear Aandrew,

    Thank you for quick response. Shared link speaks about the phase consistency between two PLL. But i am using single ADF4159 no multiple ADF4159.

    I am programming the PLL in single sawtooth burst mode and providing the external trigger pulse to TXDATA, start the ramp periodically. I required phase coherence between ramps.

    Let me know how below phase adjustment will work.

    Kindly suggest on this.

    Regards

    Sushant

  • Hi, the example I sent is for two PLLs but the same applies to consecutive chirps on one ADF4159 PLL.

    In other words the chirps are unlikely to be in the same phase due to the SDM operation. The phase resync feature is what what you need to keep the signal phase coherent between frequency changes (when in fractional N mode) and our ramping PLLs such as ADF4159 do not have this phase resync feature. If you can measure the phase on the output with external circuitry then you could use the phase adjust controls you screenshotted to manually adjust the phase at the start of each ramp. 

Reply
  • Hi, the example I sent is for two PLLs but the same applies to consecutive chirps on one ADF4159 PLL.

    In other words the chirps are unlikely to be in the same phase due to the SDM operation. The phase resync feature is what what you need to keep the signal phase coherent between frequency changes (when in fractional N mode) and our ramping PLLs such as ADF4159 do not have this phase resync feature. If you can measure the phase on the output with external circuitry then you could use the phase adjust controls you screenshotted to manually adjust the phase at the start of each ramp. 

Children
No Data