KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADAR1000
Recommended for New Designs
The ADAR1000 is a 4-channel, X and Ku frequency band, beamforming core chip for phased arrays. This device operates in half-duplex between receive and...
Datasheet
ADAR1000 on Analog.com
Hi,
I have 2x ADAR1000s and would like to daisy chain them together.
The ADAR1000 is controlled using and Arduino. The Arduino is programmed using MATLAB. The arduino is connected to boards 1's P1 pins.
Board 1's P2 connector is connected to Board 2's P1 connector.
I have also connected Position 4 to Position 6 of the P10 pinout.
My MATLAB script is the following:
%% Board 1
a = arduino();
ADAR1000 = device(a, 'SPIChipSelectPin', 'D10');
writeRead(ADAR1000, [0x00 0x00 0x81]) % Reset
writeRead(ADAR1000, [0x00 0x00 0x18]) % SPI Open
writeRead(ADAR1000, [0x00 0x38 0x60]) % VGA BIAS 2
%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
writeRead(ADAR1000, [0x00 0x2F 0x7F]) % Tx Bias
writeRead(ADAR1000, [0x00 0x36 0x16])
writeRead(ADAR1000, [0x00 0x37 0x06])
writeRead(ADAR1000, [0x00 0x31 0x42]) % Current On
%% TX1
writeRead(ADAR1000, [0x00 0x1C 157]) % Gain
writeRead(ADAR1000, [0x00 0x20 0x3F]) % I
writeRead(ADAR1000, [0x00 0x21 0x20]) % Q
%% Board 2
writeRead(ADAR1000, [0x20 0x00 0x18]) % SPI Open
writeRead(ADAR1000, [0x20 0x38 0x60]) % VGA BIAS 2
%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
writeRead(ADAR1000, [0x20 0x2F 0x7F]) % Tx Bias
writeRead(ADAR1000, [0x20 0x36 0x16])
writeRead(ADAR1000, [0x20 0x37 0x06])
writeRead(ADAR1000, [0x20 0x31 0x42]) % Current On
%% TX1
writeRead(ADAR1000, [0x20 0x1C 157]) % Gain
writeRead(ADAR1000, [0x20 0x20 0x3F]) % I
writeRead(ADAR1000, [0x20 0x21 0x20]) % Q
I have tried to address each board independently and can confirm that the addresses 0x00 and 0x20 are working.
However when I run the above script only one board seems to work. Is there anything I am missing?
Many thanks,
Zain
Which board is not responsive when daisy chained? Try observing SPI lines on the board with an oscilloscope to make sure signals are being received/sent.
Also, can you define what "work" means exactly? Are the supply currently levels correct? How about the Tx gain?
I notice that you enable the SDO pins of both parts, which you don't want to do due to a silicon error. Can you do any SPI readbacks if you only enable one SDO pin?
Also note you will need a 0x2802 write to update any changes to the gain and phase registers.