Post Go back to editing

ADF4159 Phase noise improvement

Thread Summary

The user is integrating an ADF4159 PLL evaluation board with an external HMC510LP5E VCO and a 100 MHz external clock source to generate a 30 MHz ramp signal from 9300 MHz to 9330 MHz. The phase noise in CW and FMCW modes can differ, with the reference signal dominating at low offsets, the VCO at far offsets, and the PLL's FOM in between. To improve phase noise, optimize the loop filter bandwidth and keep the PFD frequency high. Using an external VCO and OCXO can affect phase noise, and the ADIsimPLL tool can help simulate the ramp linearity and phase noise response.
AI Generated Content

Hi team,

I integrated the ADF4159 PLL evaluation board with an external VCO i.e., HMC510LP5E to generate desired frequencies for the application I'm working on. Also I'm giving the reference signal of 100MHz from an external clock source(LN100) instead of on board OCXO. I'm trying to generate a ramp signal that covers a range of 30MHz, starting from 9300 MHz to 9330MHz. I designed the loop filter by setting the PFD to 25MHz using the ADIsimPLL software. 

Now, I have few questions as follows

  1. Can the phase noise produced in ADF PLL during CW and FMCW frequencies generation be same in both cases?
  2. How do I estimate the exact phase noise in PLL I'm using?
  3. How can I improve the phase noise? Is it dependent on the loop filter design or PFD frequency setting?
  4. Does using an external VCO and OCXO affect the phase noise produced in PLL?

I'm attaching the loop design file screenshot here in case anyone wants to know the settings I set.

Thanks in advance.