Post Go back to editing

About S-parameters of LTC5532 above 7GHz

Hello

Is there data for the LTC5532 S-parameters from 7GHz to 12GHz?

I would be grateful if you could reply.

Best Regards,
Knj

Top Replies

Parents
  • Hello Knj,

    See attached file for VNA LTC5532 input impedance measurement data. 

    XLS

    The data shows the 7 to 12 GHz input impedance rotating past self-resonance as seen on the Smith chart, meaning that some custom impedance matching will be required.

    For wideband applications, it may be difficult to achieve adequate impedance match with only reactive matching elements. In this case, a combination of resistive and reactive matching elements should work well, although detector response will likely exhibit some degradation up at the higher frequencies.  -Bruce H. 

Reply
  • Hello Knj,

    See attached file for VNA LTC5532 input impedance measurement data. 

    XLS

    The data shows the 7 to 12 GHz input impedance rotating past self-resonance as seen on the Smith chart, meaning that some custom impedance matching will be required.

    For wideband applications, it may be difficult to achieve adequate impedance match with only reactive matching elements. In this case, a combination of resistive and reactive matching elements should work well, although detector response will likely exhibit some degradation up at the higher frequencies.  -Bruce H. 

Children
No Data